Other Parts Discussed in Thread: LM3406
dear
LM3406HV turns on for 1 minute, IC heats up to 70 degrees
Questions are as follows:
LM3406HV applications are as follows:
Input: 60V
Output: 54V 1.3A COB LED
When the RON resistance is set to 150K, the frequency is about 430K, and the LM3406HV heats up severely and the temperature is below 90 degrees.
When the RON resistance is set to 300K, the frequency is about 300K, and the heating temperature of LM3406HV is about 70 degrees.
Excuse me, can LM3406HV achieve 60W? How big should the RON resistance be set? What is the appropriate frequency setting?
How to solve the heating temperature of this LM3606HV?
Can I set the frequency to 120KHZ?