This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD23381F4: MOSFET Source Low voltage output

Part Number: CSD23381F4
Other Parts Discussed in Thread: CSD23382F4

Hello,

I have some problems when using P-MOSFET CSD23381F4 as a switch.

I driving the gate with  2.8v~4.2V, and provide source voltage 0V(DC3VB power off),  Drain voltage 0V .

At that time source output voltage is 0.56V not 0V (Q9- pin2 in the figure below).

=>So, please help to confirm whether the 0.56V(Vs) voltage comes from gate protection diode  ?


Under the same application conditions, is there any other TI P-MOSFET whose source output is 0V.

Thanks.