Hello expert
When I use UCD3138PFCEVM-026, I select single-phase PFC mode, the input AC is 115V, and LED3 will be red when power is on. What is the cause of the error?The load is 500 ohms.The program comes from TI's official website, no changes.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello expert
When I use UCD3138PFCEVM-026, I select single-phase PFC mode, the input AC is 115V, and LED3 will be red when power is on. What is the cause of the error?The load is 500 ohms.The program comes from TI's official website, no changes.
Hello,
Please setup the EVM following the User's Guide.
https://www.ti.com/lit/pdf/sluu885?keyMatch=SLUU885B
Does the PFC converter work normally? and is LED3 always on in full range load and full range input?
You can monitor/check the Supply State by the Memory Debugger in GUI Tool.
Regards,
Teng
A few seconds after power-on, LED3 starts to light up, and the corresponding register in the memory debugger monitor changes from 0 to 1. The code is downloaded from the official website without modification, and the input voltage is within the specified range. Why does this happen? In addition, when compiling on CCS, the following code (lines 9 and 10) will appear, saying that the specified path was not found. Does this have any effect?
**** Clean-only build of configuration UCD3138 for project PWR026_PFC **** "C:\\ti\\ccs1040\\ccs\\utils\\bin\\gmake" -k clean DEL /F "PWR026_PFC_UCD3138.hex" "PWR026_PFC_UCD3138.out" DEL /F "clear_program_flash.lst" "cyclone_global_variables_defs.lst" "flash.lst" "init_dpwms.lst" "init_filters.lst" "init_front_ends.lst" "init_loop_mux.lst" "init_miscellaneous.lst" "interrupts.lst" "loop_configurations.lst" "main.lst" "pmbus_constants.lst" "pmbus_topology.lst" "primary_secondary_communication.lst" "software_interrupt.lst" "software_interrupt_wrapper.lst" "standard_interrupt.lst" "uart.lst" "zero_out_integrity_word.lst" "Device/UCD3138/Source/load_UCD3138.lst" "Driver/Pmbus/pmbus_command_indexes.lst" "Driver/Pmbus/pmbus_common.lst" "Driver/Pmbus/pmbus_driver.lst" DEL /F "clear_program_flash.obj" "cyclone_global_variables_defs.obj" "flash.obj" "init_dpwms.obj" "init_filters.obj" "init_front_ends.obj" "init_loop_mux.obj" "init_miscellaneous.obj" "interrupts.obj" "loop_configurations.obj" "main.obj" "pmbus_constants.obj" "pmbus_topology.obj" "primary_secondary_communication.obj" "software_interrupt.obj" "software_interrupt_wrapper.obj" "standard_interrupt.obj" "uart.obj" "zero_out_integrity_word.obj" "Device\UCD3138\Source\load_UCD3138.obj" "Driver\Pmbus\pmbus_command_indexes.obj" "Driver\Pmbus\pmbus_common.obj" "Driver\Pmbus\pmbus_driver.obj" DEL /F "clear_program_flash.asm" "cyclone_global_variables_defs.asm" "flash.asm" "init_dpwms.asm" "init_filters.asm" "init_front_ends.asm" "init_loop_mux.asm" "init_miscellaneous.asm" "interrupts.asm" "loop_configurations.asm" "main.asm" "pmbus_constants.asm" "pmbus_topology.asm" "primary_secondary_communication.asm" "software_interrupt.asm" "software_interrupt_wrapper.asm" "standard_interrupt.asm" "uart.asm" "zero_out_integrity_word.asm" "Device/UCD3138/Source/load_UCD3138.asm" "Driver/Pmbus/pmbus_command_indexes.asm" "Driver/Pmbus/pmbus_common.asm" "Driver/Pmbus/pmbus_driver.asm" System can not find the route System can not find the route Finished clean **** Build Finished **** **** Build of configuration UCD3138 for project PWR026_PFC **** "C:\\ti\\ccs1040\\ccs\\utils\\bin\\gmake" -k all Building file: "../clear_program_flash.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../clear_program_flash.c" Finished building: "../clear_program_flash.c" Building file: "../cyclone_global_variables_defs.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../cyclone_global_variables_defs.c" Finished building: "../cyclone_global_variables_defs.c" Building file: "../flash.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../flash.c" Finished building: "../flash.c" Building file: "../init_dpwms.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../init_dpwms.c" Finished building: "../init_dpwms.c" Building file: "../init_filters.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../init_filters.c" Finished building: "../init_filters.c" Building file: "../init_front_ends.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../init_front_ends.c" Finished building: "../init_front_ends.c" Building file: "../init_loop_mux.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../init_loop_mux.c" Finished building: "../init_loop_mux.c" Building file: "../init_miscellaneous.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../init_miscellaneous.c" Finished building: "../init_miscellaneous.c" Building file: "../interrupts.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=32 --abi=ti_arm9_abi -O1 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../interrupts.c" Finished building: "../interrupts.c" Building file: "../loop_configurations.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../loop_configurations.c" Finished building: "../loop_configurations.c" Building file: "../main.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --preproc_with_comment --preproc_with_compile --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../main.c" Finished building: "../main.c" Building file: "../pmbus_constants.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../pmbus_constants.c" Finished building: "../pmbus_constants.c" Building file: "../pmbus_topology.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../pmbus_topology.c" Finished building: "../pmbus_topology.c" Building file: "../primary_secondary_communication.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../primary_secondary_communication.c" Finished building: "../primary_secondary_communication.c" Building file: "../software_interrupt.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=32 --abi=ti_arm9_abi -O2 --opt_for_speed=5 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../software_interrupt.c" Finished building: "../software_interrupt.c" Building file: "../software_interrupt_wrapper.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../software_interrupt_wrapper.c" Finished building: "../software_interrupt_wrapper.c" Building file: "../standard_interrupt.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=32 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../standard_interrupt.c" Finished building: "../standard_interrupt.c" Building file: "../uart.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../uart.c" Finished building: "../uart.c" Building file: "../zero_out_integrity_word.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=32 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" "../zero_out_integrity_word.c" Finished building: "../zero_out_integrity_word.c" Building file: "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Source/load_UCD3138.asm" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" --obj_directory="Device/UCD3138/Source" "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Source/load_UCD3138.asm" Finished building: "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Source/load_UCD3138.asm" Building file: "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus/pmbus_command_indexes.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" --obj_directory="Driver/Pmbus" "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus/pmbus_command_indexes.c" Finished building: "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus/pmbus_command_indexes.c" Building file: "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus/pmbus_common.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" --obj_directory="Driver/Pmbus" "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus/pmbus_common.c" Finished building: "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus/pmbus_common.c" Building file: "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus/pmbus_driver.c" Invoking: ARM Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Header" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus" --include_path="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/" -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" --obj_directory="Driver/Pmbus" "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus/pmbus_driver.c" Finished building: "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Driver/Pmbus/pmbus_driver.c" Building target: "PWR026_PFC_UCD3138.out" Invoking: ARM Linker "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 -g --define=UCD3138=1 --define=INTERLEAVED=0 --define=SINGLE_PHASE=1 --define=BRIDGELESS=2 --define=ON=1 --define=OFF=0 --define=PFC_TYPE=SINGLE_PHASE --define=EMETER_EN=OFF --define=VBUS_CHANGE_MODE=OFF --define=AC_DROP_MODE=OFF --define=AC_CYCLE_SKIP=OFF --define=HARMONIC_INJECTION=OFF --define=ZVS_CONTROL=OFF --define=DIVIDE_TABLE=OFF --define=AUTO_CAL_CURRENT_OFFSET=OFF --diag_warning=225 --display_error_number -k --asm_listing --pp_directory="D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/PFC/UCD3138_PFCEVM_026_CCS6/UCD3138" -z -m"PWR026_PFC_UCD3138.map" --stack_size=200 --heap_size=10 -i"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/lib" -i"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/include" --reread_libs --define=UCD3138=1 --display_error_number --warn_sections --xml_link_info="PWR026_PFC_linkInfo.xml" --rom_model -o "PWR026_PFC_UCD3138.out" "./clear_program_flash.obj" "./cyclone_global_variables_defs.obj" "./flash.obj" "./init_dpwms.obj" "./init_filters.obj" "./init_front_ends.obj" "./init_loop_mux.obj" "./init_miscellaneous.obj" "./interrupts.obj" "./loop_configurations.obj" "./main.obj" "./pmbus_constants.obj" "./pmbus_topology.obj" "./primary_secondary_communication.obj" "./software_interrupt.obj" "./software_interrupt_wrapper.obj" "./standard_interrupt.obj" "./uart.obj" "./zero_out_integrity_word.obj" "./Device/UCD3138/Source/load_UCD3138.obj" "./Driver/Pmbus/pmbus_command_indexes.obj" "./Driver/Pmbus/pmbus_common.obj" "./Driver/Pmbus/pmbus_driver.obj" "../ipm.lib" "../Device/UCD3138/Linker/cyclone.cmd" "D:/ti/QIU_PFC026_20210924_guanfangxiazai/PFC/Firmware/Device/UCD3138/Linker/cyclone_headers.cmd" -llibc.a <Linking> Finished building target: "PWR026_PFC_UCD3138.out" Tektronix Extended format "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_5.2.9/bin/armhex.exe" -x "PWR026_PFC_UCD3138.out" -o "PWR026_PFC_UCD3138.x0" -memwidth 8 Translating to Extended Tektronix format... "PWR026_PFC_UCD3138.out" .vectors ==> .vectors "PWR026_PFC_UCD3138.out" .text ==> .text "PWR026_PFC_UCD3138.out" .const ==> .const "PWR026_PFC_UCD3138.out" .zero_out_integrity_word_0 ==> .zero_out_integrity_word_0 "PWR026_PFC_UCD3138.out" .clear_program_flash ==> .clear_program_flash "PWR026_PFC_UCD3138.out" FixedDeviceID ==> FixedDeviceID "PWR026_PFC_UCD3138.out" .CONFIG ==> .CONFIG **** Build Finished ****
I would suggest using the Fusion Digital Power Studio Firmware to monitor the power supply and see if you get any faults reported, and just in general what the status is. If it is detecting a fault and turning on the error LED, you should be able to see it.