Hello team,
My customer will use TPS562208 in condition with Vin=12V±3%, Vout=5.97V, Iout=1.25A.
WBENCH recommends L1=3.3uH, but they want to use 6.8uH because of inductor availability. In the datasheet, max value is 4.7uH.
Can you check if they can use L1=6.8uH?
Best regards,
Shotaro