This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24702: Inquiry about VS

Part Number: BQ24702

Hello Expert,

I have some question about VS.

Could you please check and reply in line about each questions (Yellow background color)?

1. When power off, our customer want to minimize leakage current from battery.

    So they will adjust resistor value of divider circuit at VS pin.

    What's the minimum request current at VS pin?

    Here is their circuit.

    Series : 620Kohm, Shunt : 75Kohm

    They will raise value of the series resistor to reduce leakage.

    604Kohm is on the reference circuit of data sheet.

    What's the maximum value of series resistor?

    

2. About below V(vs),

   

    When BATP is 1V, if VS is within 1V ±2%, does it mean to enable BATDRV?


     For example, if the BATP is 2V, will it work if the VS is within 2V ±2%?

Best Regards,

Michael