Hello,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Sai,
It is typical to only use the needed channels and to leave the others disconnected - see datasheet section 10.2.1.2 Detailed Design Procedure for more details. I haven't seen an application where the user used multiple devices to monitor the same battery cell. My concerns are around the ability to cell balance and the potential voltage accuracy errors due to this overlapping setup.
I assume that these are on the same PCB and so I don't have any isolation or safety concerns.
Sai,
Ok in that case, then as long as the software doesn't cause a conflict then this should work. There will be some impact to accuracy however.