Hi team,
Can i use 2 MOSFET to share the current?
The rating will up to 30V 70A
Can keep using LM74700-Q1?
Sincerely.
Minki Li
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Can i use 2 MOSFET to share the current?
The rating will up to 30V 70A
Can keep using LM74700-Q1?
Sincerely.
Minki Li
Hi Mink,
Yes, LM74700-Q1 can drive more than one MOSFET in parallel. As the no. of FETs in parallel increase, the gate capacitance increases. It is important to understand the turn on time based on the gate capacitance of the total MOSFETs in parallel.
This device maximum peak gate drive current is about 11mA and turn ON time T_on = C_gate * (Vth_MOSFET) / 11mA. Note that until the MOSFET turns ON, body diode would conduct the current.