Other Parts Discussed in Thread: UCC28070,
Hi support team,
I am looking for a 2-output ACDC converter with the following specifications.
ACDC converter specifications
・AC Input Voltage Range: 85 to 264V
・DC Output 1: 60V, 10A
・DC Output 2: 12V, 30A
・Isolated : Yes
・Application: Large capacity charger
In the related question, UCC28070 was introduced as a pre-regulator that generates DC390V.
However, I am considering UCC28180 because I want to use a simple device.
We plan to generate DC390V with UCC28180 and place two UCC25640x systems in the latter stage.
Is UCC28180 suitable for this application?
Please let me know if there is another suitable IC.
Regards,
Dice-K