Other Parts Discussed in Thread: UCC28950, UCC28070, UCC28180
Hi support team,
I am looking for a 2-output ACDC converter with the following specifications.
ACDC converter specifications
・AC Input Voltage Range: 85 to 264V
・DC Output 1: 60V, 10A
・DC Output 2: 12V, 30A
・Isolated : Yes
・Application: Large capacity charger
In the related question, I am considering placing two UCC28950/1 after the PFC pre-regulator UCC28070 that generates DC390V.
However, since I want to use a simple device, I am considering generating DC390V with UCC28180 and placing two UCC25640x systems in the latter stage.
Is UCC25640x suitable for this isolated DCDC converter?
Please let me know if there is another suitable IC.
Regards,
Dice-K