We have an issue with the UCC21732 transistor driver IC. Setting the combined Enable/Reset* pin low does not clear its fault latch, as we would expect. Thorough reading of the data sheet reveals that the latch is cleared at rising edge of the En/Rst* pin.
I really don't like this. It means that we must redesign the protection logic so it allows turning on a faulty converter. This may give quite spectacular results, fireworks.
* Do you have any suggestions about how to clear the fault latch without having to turn on the power transistors?
Our design is stressed on latency so we don't want to add any logic gates in the control signal paths.
A crude workaround could be to short the 5V supply. The fault handling logic could do that by turning on a large crowbar transistor briefly, so the undervoltage/powering up logic in the driver IC would clear its fault latch.
* Is this something you would recommend, does shorting the 5V rail to clear the fault latches make sense?