Other Parts Discussed in Thread: TPA3221
Hi TI
I can't find an answer to this question anywhere so I thought I would ask it here.
I am using 2x LM5122 boost converters to create the 30V PVDD power supply for TPA3221 audio amplifier.
Should I attempt to synchronise the clocks of the TPA3221 and the LM5122?
There appears to be a 2.88Mhz clock output from the TPA3221.. I could div 8 to use this to sync the LM5122.
Is this advisable in terms of EMI/power supply noise? Or is it best to leave both clocks free running?
Also, what is the difference between LM25122 and LM5122?
Kind regards
David