This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24045: battery charger ic

Part Number: BQ24045
Other Parts Discussed in Thread: BQ25180

Hi Team,

May I ask for help regarding with our customer requirement below?

"I just want to know one thing about the battery charger ic bq2404x
we have one requirement in the project that we dont want to provide the power to the board once the setup is in charging
can we do with this ic?

i will just tell my requirment completely
we have one requirement in the project that we want to charge the battery and at that time the system will not take power from the usb i.e the system will power on only when the battery is connected. suppose the battery is not connected at that time when we connect the usb cable the system will not power on.
this is my requirement"

Is the requirement of our customer can be done with BQ24045? If yes, can you further explain how should this be done properly? Thank you so much.

Kind regards,
Gerald