Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO
I was using this studio without any issue with same IC now had to do some changes with new IC's all of them are showing "auto detected device is :0100_0_06" which is not is the list of gauges i think this is the problem.
I have tested with new BQstudio Stable version 1.3.101 with updated Chemistry version 869.
still same problem .
How to resolve this? and what will happen if i connect it with the "0100_0_16-bq34z100G1" as of now there are few registers I can't read or some i can't write, is it possible that it can damage the IC?