Other Parts Discussed in Thread: BQ25120A
to reduce power consumtion when the battery gets to its EODC voltage of 3.3V our firmware commands the FG in shutdown mode. GPout is pulled up to the system supply voltage (3.2V or 1.8V from bq25120a). When battery voltage further decreases e.g. to 3.1V the system supply voltage is completely shut of, so there is no potential on GPout. If the device is put on a charger the system supply voltage returns to 3.2V. Will this voltage rise on GPout wake the FG from shutdown? can you provide the logic levels for GPout when used as input?
Regards
Nikolaus