Dear TI
I have two questions about the "TPS7A4501" data sheet.
Please answer the following two points.
(1) The data sheet stated that the reference voltage (Vadj) was about 1.21V ± 3% under the "full range" condition. I think that the accuracy will improve when the input / output range is narrowed down to "Vin = 2.5V to 10V, Iload = 1mA to 500mA". Is this perception correct?
(2) Is there any Vadj data that specifies the input / output range more finely than the conditions described in the data sheet?
Best Regards,
Taroimo