We use UCC21710-Q1 to drive a SIC-MOSFET and use a isolation power supply to power UCC21710-Q1.. But when we power-up the board, the circuit does not work. Later it was found that the resistance between "VDD" pin and "COM" pin is very small, less than 1Ohm.. What is the root-cause for this? Is this due to power supply "VDD to COM" is to big and damage the chip?