Hello Experts,
I have same question as follows, instead output voltage is 1.9V. Do you have any way to output 1.9V by fixed output voltage version?
------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Our customer need the adjustable TPSM82822SILR but it is not available anywhere. To solve his problem for a 1.1V (which is not available as a fixed output type) output he needs some confirmation.
Can any of the TPSM82822xSILR fixed output devices be adjusted to another output voltage? His assumption is that these devices use a fixed internal resistor divider. If the resistor divider is accessible to the pins normally used by the adjustable version, then it may be possible to adjust the output voltage even though this is a fixed output type. Is his assumptions correct?
------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Best Regards,
Fujiwara