When i set input
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When i set input
Hello Minki,
The available diode library in Webench is limited. There are only few diodes with a high voltage rating. PMEG6010CEGWX is ok for Dbootx.
For Df, the current needed to drive the MOSFETs needs to be taken into account as this is coming from the input through this diode. I would use a diode with a bigger package for power dissipation reasons as long as you are not connecting VOUT to BIAS. Then the current is coming from the output and the PMEG6010CEGWX should be good enough as long as your input voltage is not going above 50V. Please keep spikes in mind.
Best regards,
Brigitte