Other Parts Discussed in Thread: LMZ31503, TPS54320
Greetings, we are attempting to track a 1.8V turn on (LMZ31506) to a 3.3V turn on (LMZ31503). The resistors we've calculated are R1 = 37.8K and R2 = 18.9K. Unfortunately this results in ~ 1.1V at the SS/TR input which result in the PWRGD signal to be pulled down since it's below 1.4V. The PWRGD signal is required to enable another regulator in the sequence. Any thoughts on an alternate method to track the two devices and enable PWRGD from the 1.8V device? Thank you