Dear Team,
The TPSM5601R5H has 26-µA non-switching quiescent current. Can you tell me what the switching quiescent current is? (Customer request)
Thanks,
Daniel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
The TPSM5601R5H has 26-µA non-switching quiescent current. Can you tell me what the switching quiescent current is? (Customer request)
Thanks,
Daniel
Hi,
Do you have the VIN and VOUT condition for the quiescent current?
Thanks
-Arief
Hi,
I measured this on the EVM at no load
at 12V input and 5V output the input current is 11.51mA
at 24V input and 5V output the input current is 14.34mA
Thank you
-Arief