Dear Sir,
I have a strange problem. I have 4 LiFePO4 cells (Vc3 and VC4 shorted on the Bq7692003), when the battery voltage is about less than 11V, sometimes I see the cells and the battery voltage read by Bq7692003 that change the values. For example I read for much seconds a 2900mV on the cell, and sometimes for 2/3 seconds I read about 2100mV. The REGSRC and BAT pins have less than 11V, there are 2 diodes. What happen?
Regards,
Davide