Hi team,
Could you clarify the behavior if VSENSE value is higher than 2.4V, but is below Ilim value?
For example,
Normal operation current = 50mA to 100mA
Short to GND > 150mA (set Rlim >150mA)
Rsense = 2.3V x 198/110mA = 4.14=3.9kohm
If 130mA current flow, Vsense = 130mA/198*3.9kohm=2.56V
which is above "Short to GND" threshold, but it doesn't hit the current limit.
In this case, switch continues ON, current limit is not triggered, /ERR is High, VSENSE is clamped n between 2.4V to 2.65V.
Is my understanding correct?
regards,