Hi experts,
A customer plans to use TPS65138 for biasing OLED. Regarding the CTRL pin, is it able to set the voltage up again after the end of adjustment? Or should it be pull-down again to disable and then send a desired number of pulse (rising edge)?
After CTRL pin is toggled to adjust voltage and keeping to be pullup, does the customer simply toggle the CTRL again to set the next voltage?
On other hands, Is it able not to output -4.9V? For example, the rising edge counting is done before the default voltage output, or there is any way to change the default output voltage. Customer want more bigger >-4.5V.
Best regards,
Hideki