I am supporting a design currently evaluating the TPS27S100.
The device is undergoing a specific evaluation, where, while the driver is ON and sourcing current, it experiences periodic Shutdown (driver output = OFF) for short intervals. The test just checks to make sure the driver output really is OFF.
Test #1:
Interval = 1[s]
OFF = 30[ms]
During this test, it seems the xFAULT signal is asserted at times. This has been confirmed by the system response, which reacts to an xFAULT condition; there is no waveform yet.
xFAULT may be asserted due to any of the following (4) points.
1) Short to GND
2) Open load, Short to supply
3) Thermal shutdown
4) Thermal swing
Assuming this has some relationship to the device overheating, is there any way to differentiate in the lab between a (3) fault, and a (4) fault?