Other Parts Discussed in Thread: BQ25175, CSD13381F4,
Hi,
I'm using a BQ29733 (-100mV / 120mV for Vocc / Vocd) to protect a VARTA CP1654 li-ion 155mAh cell battery.
The system use a 150mA charging current, and system need only 10mA (mean value).
The PACK+ will be connected to a dedicated charger, the BQ25175, connected to a USB port.
VARTA CP1654 A4 MAX DISCHARGE = 3.5CA = 542mA
VARTA CP1654 A4 MAX CHARGE = 2.5CA = 387mA
So I first selected a CSD17483FA 250mOhm FemtoFET as specified by VARTA which gave me:
With RDSon = 210mOhm (25°C, VGS 3.5V)
-> max discharge = 286mA (1.91C)
-> max charge = 238mA (1.59C)
With RDSon max = 280mOhm (25°C, VGS 3.5V)
-> max discharge = 214mA (1.43C)
-> max charge = 179mA (1.19C)
As you can see, the max value of RDSon make the max allowed charging too far from the cell capabilities and too close from the used charging current.
Am I overthinking it?
So I've moved on the 180mOhm FemtoFET CSD13381F4:
With RDSon = 150mOhm (25°C, VGS 3.5V)
-> max discharge = 400mA (2.58C)
-> max charge = 333mA (2.15C)
With RDSon max = 200mOhm (25°C, VGS 3.5V)
-> max discharge = 300mA (1.94C)
-> max charge = 250mA (1.61C)
It's better, but VDSS is 12V when the BQ2973 datasheet say 25V.
Here is my questions:
- Why it's so important to choose a MOSFET with VDSS at 25V as specified?
- Why the PACK- and V- input are given to minimal value of "BAT – 28" Volts ? Where do this "28" comes from?
- If BAT is very low, let's say 2.7V, V- can be set at 25.3V? How?
- What happen to RDSon at -10°C or 10°C? Why the datasheet only give 2 curves for RDSon at 25°C and 125°C? It would be great to have curves for at least 3 temp + all VGS rated.
Don't hesitate to ask if you have questions,
Thank you for your time.
Best regards,
Steven Valsesia