Dear Team,
Our MSP430 connects 3 PSEs,
The normal situation of the I2C address is as follows,
Port 1: I2C address is 0x20
Port 2: I2C address is 0x20
Port 3: I2C address is 0x20
Port 4: I2C address is 0x20
Port 5: I2C address is 0x20
Port 6: I2C address is 0x20
Port 7: I2C address is 0x20
Port 8: I2C address is 0x20
Port 9: I2C address is 0x22
Port 10: I2C address is 0x22
Port 11: I2C address is 0x22
Port 12: I2C address is 0x22
Port 13: I2C address is 0x22
Port 14: I2C address is 0x22
Port 15: I2C address is 0x22
Port 16: I2C address is 0x22
Port 17: I2C address is 0x24
Port 18: I2C address is 0x24
Port 19: I2C address is 0x24
Port 20: I2C address is 0x24
Port 21: I2C address is 0x24
Port 22: I2C address is 0x24
Port 23: I2C address is 0x24
Port 24: I2C address is 0x24
But if we perform a factory reset,
Then the I2C address will become as follows, (The I2C Address of PSE (slave) is messed up)
Is there a way to modify the I2C address through software from the console?
If it can’t, can’t it be solved only by burning the firmware with GUI?
Port 1: I2C addressr is 0x22
Port 2: I2C addressr is 0x22
Port 3: I2C addressr is 0x24
Port 4: I2C addressr is 0x24
Port 5: I2C addressr is 0x24
Port 6: I2C addressr is 0x24
Port 7: I2C addressr is 0x0
Port 8: I2C addressr is 0x0
Port 9: I2C addressr is 0x0
Port 10: I2C addressr is 0x0
Port 11: I2C addressr is 0x0
Port 12: I2C addressr is 0x0
Port 13: I2C addressr is 0x20
Port 14: I2C addressr is 0x20
Port 15: I2C addressr is 0x20
Port 16: I2C addressr is 0x20
Port 17: I2C addressr is 0x22
Port 18: I2C addressr is 0x22
Port 19: I2C addressr is 0x0
Port 20: I2C addressr is 0x0
Port 21: I2C addressr is 0x0
Port 22: I2C addressr is 0x0
Port 23: I2C addressr is 0x0
Port 24: I2C addressr is 0x0
If we use “save config” command to save current setting, which command can be used to restore the saved configuration to default?
Many Thanks,
Jimmy