Hello,
At the TPS274160B datasheet it is stated that the outputs are tolerant to voltage surge of 1kV over 1.2/50uSec.
At the TPS274160B EVM there are optional TVS diodes at the outputs.
The suggested TVS diodes are SMBJ36A-13-F. The Ipp of these diodes is 10.3A, which is not sufficient for 1kV / 42ohm surge. So at what scenario these TVS diodes should be used if the device is surge proof and they can't stand the surge current?
Best regard,
Asaf abraham