Hi
he customer tested the EVB TPS259474L and encountered several problems. The resistance value calculated by the ILM resistance formula There is a big gap with the actual 3334/2.5A=1.333K Actual 2.12A Shutdown 3334/3A=1.111K Actual 2.4A Shutdown Resistance on EVB 1.65K 3334/2A=1.667K Actual 1.81A Shutdown And it is powered by a power supply, the power supply is very stable Connect the EVB input 12V, the output end is connected to the load The output current will float, no matter how high the current is adjusted, it will float Take 2.12A as an example, the lowest to 2A, the highest to 2.3A will keep jumping