This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25600: VBUS_STAT value

Part Number: BQ25600

Hi Team,

Good day. We need your help to clarify the VBUS_STAT value on the datasheet for our customer. 

Readings show VBUS_STAT = 011, which is not listed in section 8.4.9 REG08, Table 15, in the datasheet. In section 8.3.3.3.2, Table 3, VBUS_STAT = 011 is listed for PSEL = low and ILIM (aka IINDPM) = 2.4 A. This corresponds to "bq25600... 010: Adapter 2.4A → PSEL LOW” in Table 15. Therefore, the presumption is that "010" is a misspelling that should read "011".

Kindly clarify the discrepancy. Thank you for your support. 

Best regards,

Jonathan