Other Parts Discussed in Thread: BQ25180
Hi Sir,
I want to ask BQ24079T safety timer setting, I saw the RTMR resistor setting range from 18Kohm to 72Kohm in the datasheet
So the max precharge time would be 72kohm x 55s/kohm = 3960 sec, that's the maximum precharge timer is 66 minutes.
Due to our charger input source is the solar panel, it will have a lower charging current when the battery charging in precharge status.
So the precharge timing will easy to trigger the safety timer to make the charger stop charging to the battery in the field side.
Could we set the larger resistor value like 400kohm to increase the safety timer to 6 hours on precharge status?
If we increase the resistor value over 72Kohm, what it will happen in the safety timer setting?
Thanks