Other Parts Discussed in Thread: UCC256303,
Hello. I'm trying to make an LLC converter with the UCC256303 and two UCC2416-2 on the secondary side. My circuit looks similar to the UCC256303 eval-board except that I have synchronous rectification. The circuit is starting up fine and I'm able to load it a little bit (but poor efficiency so far). One of my UCC24612-2 starts to behave in a strange way when I increase the load (to around 50W) and I can hear noise from my circuit. The gate drive from the misbehaving UCC24612-2 looks like the attached figure. The gate pulses become quite wide, and I can't understand how this can happen. As long as I stay at lower loads, the gate pulses look fine.
Probably my LLC circuit is causing the problems? Can you think of any reason why the UCC24612-2 would behave like this?