Other Parts Discussed in Thread: TPS65137AEVM-366
Hello Expert,
I want to clarify to set change of negative voltage and ask about TPS65137AEVM-366.
When I understand and check the data sheet like below waveform.
The sequence is first enable (CTRL first High) and then default out (-4.9V) and then I can change negative value.
Is it possible to change negative value after only default out?
Is it right?
Second,
The sequence is first enable (CTRL first High) and then I can change negative value before default out (-4.9V) within 10ms after CTRL High and then my changed value is out.
Is it possible to change negative voltage at red box period like below?
About TPS65137AEVM-366,
Is there included USB Interface Adapter in EVK like below red box?
BR,
Michael