Hi Team,
Our customer bought TPS7A78EVM-011 evaluation module and noticed that at 230Vrms input voltage and no load, the power consumption is 6.9W. Table 2 of the user's guide states that the Pstandby is 104mW when the R6 and R7 are shorted. The customer shorted R6 and connected a jumper at J5 connector to short R7 but the power consumption is still the same, 6.9W. Upon checking the top mark of the device, it is different from the one stated in the datasheet (S7A7833) as well as the part marking lookup tool. The top mark on the actual device is XA27833 as shown in the images below. Can you please confirm if it is an original TI device or an imitation? Is the device defective?
Regards,
Danilo