This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: UCC28950 minimum switching frequency in slave mode

Part Number: UCC28950

Hi,

according to the related thread "UCC28950: To know the min switching frequency and max resistance on RAB/RCD" it's possible to run at lower frequency than 50 kHz.

What is the minimum frequency at which the UCC28950 will work? Is ist possible to run at 20 or 30 kHz?

Thanks in advance

Steffen