Hello,
I have tried to check the quiescent current of the TPS7A02 in no-load condition. According to the datasheet, that is around 25 nA.
I have used the TPS7A0220PDBVR version, 2V output, SOT 23-5 package.
I have soldered the chip on a prototype SOT 23-5 breadboard compatible.
I have soldered a 0402 100nF X5R between the 2 leads VIN and GND.
I haven't soldered a decoupling capacitor at the output, having no TH capacitor with me.
I have connected an SMU Keithley 2450 on VIN, voltage mode, 3V, 1Amp compliance limit.
I have connected a multimeter Keithley DMM6500 on Vout, with 10 MOhm impedance.
Vin is connected on the breadboard to the EN pin.
No load is connected (apart from the 10 MOhm input impedance).
When starting the experience:
Vout = 2.05V --> OK
Iq around 2 mA
If I redo the experience without the multimeter connected, same results.
I don't understand why I obtain a value so high compared to the datasheet saying it should be 25 nA.
Thanks for the help.
Regards,
Julien