Hello,
I have 3 urgent questions on the TPS7H1101A-SP.
1 Is it ok to connect the CS pin directly to VIN instead of using a pullup? We do not need to measure current.
2 Our load is less than 100ma. Given this light load, do you see any issues with having capacitance on Vin of 2uF, and capacitance on VOUT of 2uF. Can this be accurately tested with the TINA model?
3 Can you share what the gain bandwidth is for this LDO? We may have transients on the input and we are concerned about the LDO regulating fast enough. Can this be accurately tested with the TINA model?
Thanks,
Adam