Hi, BQ24800 support team,
I'm seeing some confusing waves when I used BQ24800EVM,can you briefly describe the process for me? Thanks!
As the follow figure, I set BAT=6V (DC voltage source), Battery regulation 6.288V, SYSMIN 8.8V with 2.4V offset, working in battery only boost mode.
Then, plug in 21V adapter and I can see about 0.5A charge current to battery (Charge current set 1A in register).
So, Why are there 0.5A charge current when plug in adapter?
Thanks
Harvey