Other Parts Discussed in Thread: BQSTUDIO
I have a battery connected to the BQ34Z100-G1 as shown in the datasheet. I have performed a successful learning cycle (update status has changed to 6). I currently have a few concerns:
1. The SOC will show 0% until at least one full charge and discharge has been performed. Not sure if this is normal operation
2. When I unplugged the charger when it wasn't at full the SOC jumped back down to 0%. When I plugged it back in it started going up again, but assumed that the point where I unplugged the charger was 0%.
3. While charging, at some point the SOC showed as 100% even though it wasn't. I unplugged and plugged the charger back in and the SOC jumped back down to 0% and showed 0% until the battery was fully discharged.
TLDR I'm having trouble maintaining the correct SOC. It seems to reset to 0% whenever the charger is plugged in and only seems to show accurate SOC when charging. Also, if it gets stuck at 0% even though it's at half capacity, the SOC won't update until full discharge. Is there a fix for this?