I am planning to use the BQ25505 with multiple solar cells in parallel. Should there be any reverse protection between the cells? like the diagram below?
Thanks for your help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am planning to use the BQ25505 with multiple solar cells in parallel. Should there be any reverse protection between the cells? like the diagram below?
Thanks for your help.
Hi Michael,
If the cells can be user interchanged and there is a risk of reverse install, then yes. Keep in mind the average input current to the BQ25505 is 110mA (peak inductor current of 220mA) so if, for example, each cell provides 50mA, four is parallel provides 200mA, which is more average current than the BQ25505 will accept.
Regards,
Jeff
Thanks Jeff,
Will this be an issue if I connect a source that can provide 400mA? will it damage the device or will the BQ25505 limit the current?
Hi Michael,
The BQ25505 limits the current. No damage expected.
Regards,
Jeff