Other Parts Discussed in Thread: TPS65216, TPS65218
Hi,
I am using the part TPS65218D0 in the design. However I would like to have a second source for this which would be TPS65216D0. To be able to use the later, I am going to connect below pins in TPS65218D0 to ground or make NC to accommodate with TPS65216D0.
GND- pins: 20-24, 30-33, 25, 27
NC, pins: 18, 19, 34
Any issues with these pins in TPS65218D0 to be connected as listed above?
/BR