hi team,
The customer uses LP8861-Q1 and their spec is as follows:
Vin-min=9V
Vboost= 37V
Iout= 100mA*3
current ripple 30%
f=330kHz
The recommend inductor is 22uH. But, the calculated value is 125.9uH, which is much higher than the recommend value.
Could you please explain why the recommend value is much smaller?
regards,
Cathy