This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5907-Q1: LP590725QDQNRQ1 input voltage

Part Number: LP5907-Q1

Hi Team,

There is a good new that we DIN LP590725QDQNRQ1

I want to confirm the following question

When the output voltage of LP590725QDQNRQ1 is 2.5V, the input voltage must be at least 3.5V, right? The specification is written like this,THX

  • Hi Kygo,

    The maximum dropout at max load and across temperature is spec'd at 250mV, so normally all that would be required is to have VIN > VOUT + 0.25V under all operating conditions. However, since the datasheet specifies to use this LDO with VIN >= VOUT + 1V, that is what should be followed. That is not to say that it will not work with VIN < VOUT + 1V -- it may just be that there is some undesired behavior when this condition is not met.

    Regards,

    Nick