Hi all,
I want to know the output voltage ripple of TPS62813-Q1 ? Is there relevant data?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I want to know the output voltage ripple of TPS62813-Q1 ? Is there relevant data?
thanks
Hi,
In the datasheet of the TPS62813-Q1 in section "10.2.3 Application Curves" Figure 10-42 to 10-51 is all about output voltage ripple in the two different modes PFM/PWM and also for different output voltages.
exp:
Kind Regards,
Alex
Hi Alex,
I can't tell from this waveform whether there are more than 5% or 3% spec.
Does the lab have data?
thanks
Hi Alex,
I can't tell from this waveform whether there are more than 5% or 3% spec.
Does the lab have data?
thanks
Hi Hazel,
Could you share the test conditions? Vin, Vout and the Iout range?
With that we could measure the ripple in the lab and share with you the results.
Regards,
Alex
Hi Alex,
condition 1 :Vin=5V,Vout=3.3V,I=0.7A~1A pass: 3.3*0.95<Vripple<3.3*1.05
condition 1 :Vin=5V,Vout=1.05V,I=2.24A~3.2A pass: 1.05*0.95<Vripple<1.05*1.05
thanks
Hi Hazel,
Thanks for sharing the test conditions.
I will share with you the measurement results as soon as possible.
Regards,
Alex
Hi Hazel,
This is our measurement for Vin=5V,Vout=1.05V,I=2.24A~3.2A pass: 1.05*0.95<Vripple<1.05*1.05
As you can see below the ripple was 10mV
This is our measurement for Vin=5V,Vout=3.3V,I=0.7A~1A pass: 3.3*0.95<Vripple<3.3*1.05
The ripple here was 9mV
If you need data on other testing conditions you could also use WEBENCH and simulate it this will give you a good simulation.
Kind regards,
Alex