This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM33606: Module not working

Part Number: LMZM33606

Hi Team, 

we are using LMZM33606RLXR in our board

Project: Test Equipment 

Module 1: 30V to 5V (Default 4.5V, in parallel resistance concept we will achieve 5V and 5.5V)

Module 2: 30V to 12V (Default 11.5V, in parallel resistance concept we will achieve 12V and 12.5V)

For more details refer the schematic.

Module 1 is working and we are getting expected voltage range.

Module 2 is not working and we are not getting any clue why this module is not working. 

we compared the each pin impedance w.r.t GND. Both looks same not difference.

Can you help us to troubleshoot the module.

Few Observation

Module 2: output voltage measured 1.7V to 2.01V and FB voltage in mV

Module 1: Output voltage measured 4.5V and FB voltage 1.007V