Hi Team,
we are using LMZM33606RLXR in our board
Project: Test Equipment
Module 1: 30V to 5V (Default 4.5V, in parallel resistance concept we will achieve 5V and 5.5V)
Module 2: 30V to 12V (Default 11.5V, in parallel resistance concept we will achieve 12V and 12.5V)
For more details refer the schematic.
Module 1 is working and we are getting expected voltage range.
Module 2 is not working and we are not getting any clue why this module is not working.
we compared the each pin impedance w.r.t GND. Both looks same not difference.
Can you help us to troubleshoot the module.
Few Observation
Module 2: output voltage measured 1.7V to 2.01V and FB voltage in mV
Module 1: Output voltage measured 4.5V and FB voltage 1.007V