Hello,
I'am currently designing a circuit where I need to enable/disable the 3.3V output from LMZ14203 when an external enable signal is put high. I thought on using the ENABLE PIN for that purpose but I failed to understand how this PIN works because what the datasheet is all about is how to set external resistors and capacitors for UVLO and soft start operations. This is an example of what I had in mind, when the external enable signal is high, EN = 0. But I don't know what happens at this point, the datasheet doesn't mention it. Will the output be 0V? And then, what will happen after the external enable signal is put low? Will the LMZ14203 start an UVLO operation?
Regards.