Hello
How to output 80A at 0.5V using TPS546D24AEVM-2PH?
Could you provide config file for output 80A at 0.5V?
Best regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
How to output 80A at 0.5V using TPS546D24AEVM-2PH?
Could you provide config file for output 80A at 0.5V?
Best regards.
Hello,
This product is set to only output at 0.8V. Using the TI Fusion Digital Power Designer, you may be able to margin and trim the output voltage to get as close to 0.5V as possible.
More information on the software mentioned above can be found on page ten of the EVM user guide.
Thanks,
Caleb
Hi Caleb
Thanks for your support
I tested 80A at 0.5V using TI Fusion Digital Power Designer.
However, as shown in the picture below, the current is output up to 61A and the voltage of ph2 is also unbalanced.
How to I do for output 80A at 0.5V?
Best regards
Hi Louis,
I took a 2-PH TOS546D24A EVM onto the bench and ran it at 0.5Vout and 80A. At 80A of current draw, I confirmed it on the monitor window of the Fusion software. Attached are the pertinent files for the Fusion GUI:
<?xml version="1.0" encoding="utf-8"?> <ProjectData xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xmlns:xsd="http://www.w3.org/2001/XMLSchema"> <Version>1</Version> <Timestamp>2021-10-27T16:27:44.7945025-05:00</Timestamp> <Creator>Texas Instruments Fusion Digital Power Designer v7.6.5.3.Alpha (For WCM testing) [2021-05-19]</Creator> <Devices> <Device> <PartID>TPS546D24A</PartID> <Address>36</Address> <Is_Offline>false</Is_Offline> <SAA_Number>1</SAA_Number> <Saved_In_Offline_Mode>false</Saved_In_Offline_Mode> <Saved_While_NVM_Write_Pending>true</Saved_While_NVM_Write_Pending> <Write_Protected>false</Write_Protected> <Package>0</Package> <Num_Outputs>1</Num_Outputs> <Parameters> <Parameter> <ID>VOUT_MODE</ID> <Code>32</Code> <IDAndCode>VOUT_MODE [0x20]</IDAndCode> <ValueText>Relative; EXP =-9</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x97" /> <ParameterType>Custom</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>CAPABILITY</ID> <Code>25</Code> <IDAndCode>CAPABILITY [0x19]</IDAndCode> <ValueText>Max Bus: 1000 Khz; PEC: Yes; SMBALERT#: Yes</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0xD0" /> <ParameterType>Custom</ParameterType> <ParameterCategory>Manufacturer</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_USER_DATA_01</ID> <Code>177</Code> <IDAndCode>COMPENSATION_CONFIG [0xB1]</IDAndCode> <ValueText>SEL_GMV: 1; SEL_GMI: 2; SEL_RVV: 8; SEL_INTV: 3; SEL_CPV: 3; SEL_RVI: 8; SEL_INTI: 9; SEL_CPI: 3; SEL_RINTI: 0;</ValueText> <ValueEncoded xsi:type="PMBusBlock" Hex="0x1220C62246" /> <ParameterType>Raw</ParameterType> <ParameterCategory>User</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>FREQUENCY_SWITCH</ID> <Code>51</Code> <IDAndCode>FREQUENCY_SWITCH [0x33]</IDAndCode> <ValueText>550 kHz</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0226" /> <ValueNumeric>550</ValueNumeric> <ParameterType>Frequency</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IC_DEVICE_ID</ID> <Code>173</Code> <IDAndCode>IC_DEVICE_ID [0xAD]</IDAndCode> <ValueText>0x5449546D2441 (TPS546D24A)</ValueText> <ValueEncoded xsi:type="PMBusBlock" Hex="0x5449546D2441" /> <ParameterType>Raw</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IC_DEVICE_REV</ID> <Code>174</Code> <IDAndCode>IC_DEVICE_REV [0xAE]</IDAndCode> <ValueText>0x4000</ValueText> <ValueEncoded xsi:type="PMBusBlock" Hex="0x4000" /> <ParameterType>Raw</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_INTERLEAVE</ID> <Code>55</Code> <IDAndCode>INTERLEAVE [0x37]</IDAndCode> <ValueText>Group ID: 0; Num Group: 2; Interleave Order: 0 (0°)</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0020" /> <ParameterType>Custom</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_CAL_GAIN</ID> <Code>56</Code> <IDAndCode>IOUT_CAL_GAIN phase ALL [0x38]</IDAndCode> <ValueText>1.090 </ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xC88C" /> <ValueNumeric>1.09</ValueNumeric> <ParameterType>Ratio</ParameterType> <ParameterCategory>Calibration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_CAL_OFFSET</ID> <Code>57</Code> <IDAndCode>IOUT_CAL_OFFSET phase ALL [0x39]</IDAndCode> <ValueText>0.0000 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xE000" /> <ValueNumeric>0</ValueNumeric> <ParameterType>CurrentCalibration</ParameterType> <ParameterCategory>Calibration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_OC_FAULT_LIMIT</ID> <Code>70</Code> <IDAndCode>IOUT_OC_FAULT_LIMIT phase ALL [0x46]</IDAndCode> <ValueText>104.00 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF8D0" /> <ValueNumeric>104</ValueNumeric> <ParameterType>Current</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_OC_FAULT_RESPONSE</ID> <Code>71</Code> <IDAndCode>IOUT_OC_FAULT_RESPONSE phase ALL [0x47]</IDAndCode> <ValueText>Response=3,Restart=7,Delay=7</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0xFF" /> <ParameterType>Custom</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_OC_WARN_LIMIT</ID> <Code>74</Code> <IDAndCode>IOUT_OC_WARN_LIMIT phase ALL [0x4A]</IDAndCode> <ValueText>80.00 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF8A0" /> <ValueNumeric>80</ValueNumeric> <ParameterType>Current</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>MFR_ID</ID> <Code>153</Code> <IDAndCode>MFR_ID [0x99]</IDAndCode> <ValueText /> <ValueEncoded xsi:type="PMBusBlock" Hex="0x000000" /> <ParameterType>String</ParameterType> <ParameterCategory>Manufacturer</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>MFR_MODEL</ID> <Code>154</Code> <IDAndCode>MFR_MODEL [0x9A]</IDAndCode> <ValueText /> <ValueEncoded xsi:type="PMBusBlock" Hex="0x000000" /> <ParameterType>String</ParameterType> <ParameterCategory>Manufacturer</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>MFR_REVISION</ID> <Code>155</Code> <IDAndCode>MFR_REVISION [0x9B]</IDAndCode> <ValueText /> <ValueEncoded xsi:type="PMBusBlock" Hex="0x000000" /> <ParameterType>String</ParameterType> <ParameterCategory>Manufacturer</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>MFR_SERIAL</ID> <Code>158</Code> <IDAndCode>MFR_SERIAL [0x9E]</IDAndCode> <ValueText /> <ValueEncoded xsi:type="PMBusBlock" Hex="0x000000" /> <ParameterType>String</ParameterType> <ParameterCategory>Manufacturer</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_MFR_SPECIFIC_29</ID> <Code>237</Code> <IDAndCode>MISC_OPTIONS [MFR 29,0xED]</IDAndCode> <ValueText>PEC: False; Reset Vout: 0; Reset#: False; Vout Source: 0; Fault Count: False; ADC Resolution: 12; PullUp#: False</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0000" /> <ParameterType>UnitlessZeroDigit</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_MFR_SPECIFIC_32</ID> <Code>240</Code> <IDAndCode>NVM_CHECKSUM [MFR 32,0xF0]</IDAndCode> <ValueText>Checksum: 1F1C</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x1F1C" /> <ParameterType>UnitlessZeroDigit</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>ON_OFF_CONFIG</ID> <Code>2</Code> <IDAndCode>ON_OFF_CONFIG phase ALL [0x02]</IDAndCode> <ValueText>Mode: CONTROL Pin Only; Control: Active High, Turn off Immediately</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x17" /> <ParameterType>Custom</ParameterType> <ParameterCategory>OnOff</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>OPERATION</ID> <Code>1</Code> <IDAndCode>OPERATION [0x01]</IDAndCode> <ValueText>Unit: ImmediateOff; Margin: None (IgnoreFault)</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x04" /> <ParameterType>Custom</ParameterType> <ParameterCategory>OnOff</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>OT_FAULT_LIMIT</ID> <Code>79</Code> <IDAndCode>OT_FAULT_LIMIT phase ALL [0x4F]</IDAndCode> <ValueText>150 °C</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0096" /> <ValueNumeric>150</ValueNumeric> <ParameterType>Temperature</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>OT_FAULT_RESPONSE</ID> <Code>80</Code> <IDAndCode>OT_FAULT_RESPONSE phase ALL [0x50]</IDAndCode> <ValueText>Response=2,Restart=7,Delay=4</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0xBC" /> <ParameterType>Custom</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>OT_WARN_LIMIT</ID> <Code>81</Code> <IDAndCode>OT_WARN_LIMIT phase ALL [0x51]</IDAndCode> <ValueText>125 °C</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x007D" /> <ValueNumeric>125</ValueNumeric> <ParameterType>Temperature</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_MFR_SPECIFIC_19</ID> <Code>227</Code> <IDAndCode>PGOOD_CONFIG [MFR 19,0xE3]</IDAndCode> <ValueText>PGood On Delay: 0, PGood Off Delay: 0; OVF Mask: True; OVW Mask: False; UVW Mask: False; UVF Mask: True; OCW Mask: True; OCF Mask: True; OTW Mask: True; OTF Mask: True</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x009F" /> <ParameterType>UnitlessZeroDigit</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_MFR_SPECIFIC_30</ID> <Code>238</Code> <IDAndCode>PIN_DETECT_OVERRIDE [MFR 30,0xEE]</IDAndCode> <ValueText>Stack Config: True; Sync Config: True; Transient Reduction: True; Compensation: True; PMBus Address: True; Interleave: True;Fault Response: False; Ton Rise: True; Iout OC Fault Limit/Warn: True; Frequency Switch: True; Vout Command/Scale Loop: False</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x1F2E" /> <ParameterType>UnitlessZeroDigit</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>PMBUS_REVISION</ID> <Code>152</Code> <IDAndCode>PMBUS_REVISION [0x98]</IDAndCode> <ValueText>1.3,1.3 - Part I: 1.3, Part II: 1.3</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x33" /> <ParameterType>Custom</ParameterType> <ParameterCategory>Manufacturer</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_USER_DATA_05</ID> <Code>181</Code> <IDAndCode>POWER_STAGE_CONFIG [0xB5]</IDAndCode> <ValueText>Gate Voltage: 4.7V;</ValueText> <ValueEncoded xsi:type="PMBusBlock" Hex="0x70" /> <ParameterType>Raw</ParameterType> <ParameterCategory>User</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_IOUT</ID> <Code>140</Code> <IDAndCode>READ_IOUT phase ALL [0x8C]</IDAndCode> <ValueText>80.88 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xEA87" /> <ValueNumeric>80.88</ValueNumeric> <ParameterType>Current</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_TEMPERATURE_1</ID> <Code>141</Code> <IDAndCode>READ_TEMPERATURE_1 phase ALL [0x8D]</IDAndCode> <ValueText>76 °C</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x004C" /> <ValueNumeric>76</ValueNumeric> <ParameterType>Temperature</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_VIN</ID> <Code>136</Code> <IDAndCode>READ_VIN phase ALL [0x88]</IDAndCode> <ValueText>11.969 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xD2FE" /> <ValueNumeric>11.969</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_VOUT</ID> <Code>139</Code> <IDAndCode>READ_VOUT phase ALL [0x8B]</IDAndCode> <ValueText>0.500000 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0100" /> <ValueNumeric>0.5</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_MFR_SPECIFIC_33</ID> <Code>241</Code> <IDAndCode>SIMULATE_FAULT [MFR 33,0xF1]</IDAndCode> <ValueText>Persist Fault: False; Temp OTF: False; Iout OCF: False; Vin Off: False; Vin OVF: False; Vout UVF: False; Vout OVF: False; Persist Warn: False; Iout OCW: False; Vin UVW: False; Vin OVW: False; Vout UVW: False; Vout OVW: False</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0000" /> <ParameterType>UnitlessZeroDigit</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_MFR_SPECIFIC_31</ID> <Code>239</Code> <IDAndCode>SLAVE_ADDRESS [MFR 31,0xEF]</IDAndCode> <ValueText>Address: 0x24 (36d)</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x24" /> <ParameterType>UnitlessZeroDigit</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>SMBALERT_MASK_CML</ID> <Code>27</Code> <IDAndCode>SMBALERT_MASK_CML [0x1B]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>SMBALERT_MASK_INPUT</ID> <Code>27</Code> <IDAndCode>SMBALERT_MASK_INPUT [0x1B]</IDAndCode> <ValueText>UNIT_OFF_FOR_INSUFFICIENT_VIN,VIN_UV_WARN,VIN_OV_WARN,VIN_OV_FAULT</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0xE8" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>SMBALERT_MASK_IOUT</ID> <Code>27</Code> <IDAndCode>SMBALERT_MASK_IOUT [0x1B]</IDAndCode> <ValueText>CURRENT_SHARE_FAULT,IOUT_UC_FAULT</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x18" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>SMBALERT_MASK_MFR_SPECIFIC</ID> <Code>27</Code> <IDAndCode>SMBALERT_MASK_MFR_SPECIFIC [0x1B]</IDAndCode> <ValueText>MFR1,MFR6</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x42" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>SMBALERT_MASK_OTHER</ID> <Code>27</Code> <IDAndCode>SMBALERT_MASK_OTHER [0x1B]</IDAndCode> <ValueText>RESERVED0</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x01" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>SMBALERT_MASK_TEMPERATURE</ID> <Code>27</Code> <IDAndCode>SMBALERT_MASK_TEMPERATURE [0x1B]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>SMBALERT_MASK_VOUT</ID> <Code>27</Code> <IDAndCode>SMBALERT_MASK_VOUT [0x1B]</IDAndCode> <ValueText>TOFF_MAX_WARN</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x02" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_MFR_SPECIFIC_28</ID> <Code>236</Code> <IDAndCode>STACK_CONFIG [MFR 28,0xEC]</IDAndCode> <ValueText>Bcx Stop: 1; Bcx Start: 0</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0001" /> <ParameterType>UnitlessZeroDigit</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_BYTE</ID> <Code>120</Code> <IDAndCode>STATUS_BYTE [0x78]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_CML</ID> <Code>126</Code> <IDAndCode>STATUS_CML [0x7E]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_INPUT</ID> <Code>124</Code> <IDAndCode>STATUS_INPUT [0x7C]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_IOUT</ID> <Code>123</Code> <IDAndCode>STATUS_IOUT [0x7B]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_MFR_SPECIFIC</ID> <Code>128</Code> <IDAndCode>STATUS_MFR_SPECIFIC [0x80]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_OTHER</ID> <Code>127</Code> <IDAndCode>STATUS_OTHER [0x7F]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_TEMPERATURE</ID> <Code>125</Code> <IDAndCode>STATUS_TEMPERATURE [0x7D]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_VOUT</ID> <Code>122</Code> <IDAndCode>STATUS_VOUT [0x7A]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_WORD</ID> <Code>121</Code> <IDAndCode>STATUS_WORD [0x79]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0000" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_MFR_SPECIFIC_20</ID> <Code>228</Code> <IDAndCode>SYNC_CONFIG [MFR 20,0xE4]</IDAndCode> <ValueText>SYNC_DIR: Auto Detect SYNC (0x03); SYNC_EDGE: Synchronize to rising edge of SYNC (True))</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0xF0" /> <ParameterType>UnitlessZeroDigit</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TPSCATFISH_MFR_SPECIFIC_00</ID> <Code>208</Code> <IDAndCode>TELEMETRY_CONFIG [MFR 00,0xD0]</IDAndCode> <ValueText>VOUT: Priority: 0x00; Avg_Num: 0x03;IOUT: Priority: 0x00; Avg_Num: 0x03;TEMPERATURE: Priority: 0x00; Avg_Num: 0x03;VIN: Priority: 0x00; Avg_Num: 0x03</ValueText> <ValueEncoded xsi:type="PMBusBlock" Hex="0x030303030003" /> <ParameterType>Raw</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TOFF_DELAY</ID> <Code>100</Code> <IDAndCode>TOFF_DELAY [0x64]</IDAndCode> <ValueText>0.0 ms</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF800" /> <ValueNumeric>0</ValueNumeric> <ParameterType>TimeOneDigitMilliseconds</ParameterType> <ParameterCategory>OnOff</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TOFF_FALL</ID> <Code>101</Code> <IDAndCode>TOFF_FALL [0x65]</IDAndCode> <ValueText>0.50 ms</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF002" /> <ValueNumeric>0.5</ValueNumeric> <ParameterType>TimeOneDigitMilliseconds</ParameterType> <ParameterCategory>OnOff</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TON_DELAY</ID> <Code>96</Code> <IDAndCode>TON_DELAY [0x60]</IDAndCode> <ValueText>0.0 ms</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF800" /> <ValueNumeric>0</ValueNumeric> <ParameterType>TimeOneDigitMilliseconds</ParameterType> <ParameterCategory>OnOff</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TON_MAX_FAULT_LIMIT</ID> <Code>98</Code> <IDAndCode>TON_MAX_FAULT_LIMIT [0x62]</IDAndCode> <ValueText><No Limit></ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF800" /> <ValueNumeric>0</ValueNumeric> <ParameterType>TimeOneDigitMilliseconds</ParameterType> <ParameterCategory>OnOff</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TON_MAX_FAULT_RESPONSE</ID> <Code>99</Code> <IDAndCode>TON_MAX_FAULT_RESPONSE [0x63]</IDAndCode> <ValueText>Response=0,Restart=7,Delay=3</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x3B" /> <ParameterType>Custom</ParameterType> <ParameterCategory>OnOff</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>TON_RISE</ID> <Code>97</Code> <IDAndCode>TON_RISE [0x61]</IDAndCode> <ValueText>3.00 ms</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF00C" /> <ValueNumeric>3</ValueNumeric> <ParameterType>TimeOneDigitMilliseconds</ParameterType> <ParameterCategory>OnOff</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VIN_OFF</ID> <Code>54</Code> <IDAndCode>VIN_OFF phase ALL [0x36]</IDAndCode> <ValueText>2.50 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF00A" /> <ValueNumeric>2.5</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VIN_ON</ID> <Code>53</Code> <IDAndCode>VIN_ON phase ALL [0x35]</IDAndCode> <ValueText>2.75 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF00B" /> <ValueNumeric>2.75</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VIN_OV_FAULT_LIMIT</ID> <Code>85</Code> <IDAndCode>VIN_OV_FAULT_LIMIT [0x55]</IDAndCode> <ValueText>21 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0015" /> <ValueNumeric>21</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VIN_OV_FAULT_RESPONSE</ID> <Code>86</Code> <IDAndCode>VIN_OV_FAULT_RESPONSE [0x56]</IDAndCode> <ValueText>Response=0,Restart=7,Delay=4</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x3C" /> <ParameterType>Custom</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VIN_UV_WARN_LIMIT</ID> <Code>88</Code> <IDAndCode>VIN_UV_WARN_LIMIT [0x58]</IDAndCode> <ValueText>2.50 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF00A" /> <ValueNumeric>2.5</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_COMMAND</ID> <Code>33</Code> <IDAndCode>VOUT_COMMAND [0x21]</IDAndCode> <ValueText>0.501953 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0101" /> <ValueNumeric>0.501953125</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_MARGIN_HIGH</ID> <Code>37</Code> <IDAndCode>VOUT_MARGIN_HIGH [0x25]</IDAndCode> <ValueText>0.527443 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x021A" /> <ValueNumeric>0.527442932128906</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_MARGIN_LOW</ID> <Code>38</Code> <IDAndCode>VOUT_MARGIN_LOW [0x26]</IDAndCode> <ValueText>0.476463 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x01E6" /> <ValueNumeric>0.476463317871094</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_MAX</ID> <Code>36</Code> <IDAndCode>VOUT_MAX [0x24]</IDAndCode> <ValueText>1.500000 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0300" /> <ValueNumeric>1.5</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_MIN</ID> <Code>43</Code> <IDAndCode>VOUT_MIN [0x2B]</IDAndCode> <ValueText>0.500000 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0100" /> <ValueNumeric>0.5</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_OV_FAULT_LIMIT</ID> <Code>64</Code> <IDAndCode>VOUT_OV_FAULT_LIMIT [0x40]</IDAndCode> <ValueText>0.576462 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x024C" /> <ValueNumeric>0.576461791992188</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_OV_FAULT_RESPONSE</ID> <Code>65</Code> <IDAndCode>VOUT_OV_FAULT_RESPONSE [0x41]</IDAndCode> <ValueText>Response=2,Restart=7,Delay=5</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0xBD" /> <ParameterType>Custom</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_OV_WARN_LIMIT</ID> <Code>66</Code> <IDAndCode>VOUT_OV_WARN_LIMIT [0x42]</IDAndCode> <ValueText>0.547050 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x022E" /> <ValueNumeric>0.547050476074219</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_SCALE_LOOP</ID> <Code>41</Code> <IDAndCode>VOUT_SCALE_LOOP [0x29]</IDAndCode> <ValueText>0.500 </ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xC840" /> <ValueNumeric>0.5</ValueNumeric> <ParameterType>UnitlessThreeDigit</ParameterType> <ParameterCategory>Calibration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_TRANSITION_RATE</ID> <Code>39</Code> <IDAndCode>VOUT_TRANSITION_RATE [0x27]</IDAndCode> <ValueText>1.0000 mV/μs</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xE010" /> <ValueNumeric>1</ValueNumeric> <ParameterType>Transition</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_TRIM</ID> <Code>34</Code> <IDAndCode>VOUT_TRIM [0x22]</IDAndCode> <ValueText>0.000000 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0000" /> <ValueNumeric>0</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Calibration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_UV_FAULT_LIMIT</ID> <Code>68</Code> <IDAndCode>VOUT_UV_FAULT_LIMIT [0x44]</IDAndCode> <ValueText>0.426464 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x01B3" /> <ValueNumeric>0.426464080810547</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_UV_FAULT_RESPONSE</ID> <Code>69</Code> <IDAndCode>VOUT_UV_FAULT_RESPONSE [0x45]</IDAndCode> <ValueText>Response=2,Restart=7,Delay=6</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0xBE" /> <ParameterType>Custom</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>VOUT_UV_WARN_LIMIT</ID> <Code>67</Code> <IDAndCode>VOUT_UV_WARN_LIMIT [0x43]</IDAndCode> <ValueText>0.456856 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x01D2" /> <ValueNumeric>0.456855773925781</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>WRITE_PROTECT</ID> <Code>16</Code> <IDAndCode>WRITE_PROTECT [0x10]</IDAndCode> <ValueText>0</ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Raw</ParameterType> <ParameterCategory>Configuration</ParameterCategory> <Page>255</Page> <Phase xsi:nil="true" /> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_CAL_GAIN_1</ID> <Code>56</Code> <IDAndCode>IOUT_CAL_GAIN_1 [0x38]</IDAndCode> <ValueText>1.000 </ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xC880" /> <ValueNumeric>1</ValueNumeric> <ParameterType>Ratio</ParameterType> <ParameterCategory>Calibration</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_CAL_OFFSET_1</ID> <Code>57</Code> <IDAndCode>IOUT_CAL_OFFSET phase 1 (0x00) [0x39]</IDAndCode> <ValueText>0.0000 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xE000" /> <ValueNumeric>0</ValueNumeric> <ParameterType>CurrentCalibration</ParameterType> <ParameterCategory>Calibration</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_OC_FAULT_LIMIT_1</ID> <Code>70</Code> <IDAndCode>IOUT_OC_FAULT_LIMIT phase 1 (0x00) [0x46]</IDAndCode> <ValueText>52.00 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF0D0" /> <ValueNumeric>52</ValueNumeric> <ParameterType>Current</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_OC_WARN_LIMIT_1</ID> <Code>74</Code> <IDAndCode>IOUT_OC_WARN_LIMIT phase 1 (0x00) [0x4A]</IDAndCode> <ValueText>40.00 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF0A0" /> <ValueNumeric>40</ValueNumeric> <ParameterType>Current</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>OT_FAULT_LIMIT_1</ID> <Code>79</Code> <IDAndCode>OT_FAULT_LIMIT phase 1 (0x00) [0x4F]</IDAndCode> <ValueText>150 °C</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0096" /> <ValueNumeric>150</ValueNumeric> <ParameterType>Temperature</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>OT_WARN_LIMIT_1</ID> <Code>81</Code> <IDAndCode>OT_WARN_LIMIT phase 1 (0x00) [0x51]</IDAndCode> <ValueText>125 °C</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x007D" /> <ValueNumeric>125</ValueNumeric> <ParameterType>Temperature</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_IOUT_1</ID> <Code>140</Code> <IDAndCode>READ_IOUT phase 1 (0x00) [0x8C]</IDAndCode> <ValueText>40.63 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xE28A" /> <ValueNumeric>40.63</ValueNumeric> <ParameterType>Current</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_TEMPERATURE_1_1</ID> <Code>141</Code> <IDAndCode>READ_TEMPERATURE_1 phase 1 (0x00) [0x8D]</IDAndCode> <ValueText>77 °C</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xEA64" /> <ValueNumeric>77</ValueNumeric> <ParameterType>Temperature</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_VIN_1</ID> <Code>136</Code> <IDAndCode>READ_VIN phase 1 (0x00) [0x88]</IDAndCode> <ValueText>11.969 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xD2FE" /> <ValueNumeric>11.969</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_VOUT_1</ID> <Code>139</Code> <IDAndCode>READ_VOUT phase 1 (0x00) [0x8B]</IDAndCode> <ValueText>0.500000 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0100" /> <ValueNumeric>0.5</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_CML_1</ID> <Code>126</Code> <IDAndCode>STATUS_CML_1 [0x7E]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_INPUT_1</ID> <Code>124</Code> <IDAndCode>STATUS_INPUT_1 [0x7C]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_IOUT_1</ID> <Code>123</Code> <IDAndCode>STATUS_IOUT_1 [0x7B]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_MFR_SPECIFIC_1</ID> <Code>128</Code> <IDAndCode>STATUS_MFR_SPECIFIC_1 [0x80]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_TEMPERATURE_1</ID> <Code>125</Code> <IDAndCode>STATUS_TEMPERATURE_1 [0x7D]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>0</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_CAL_GAIN_2</ID> <Code>56</Code> <IDAndCode>IOUT_CAL_GAIN_2 [0x38]</IDAndCode> <ValueText>1.000 </ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xC880" /> <ValueNumeric>1</ValueNumeric> <ParameterType>Ratio</ParameterType> <ParameterCategory>Calibration</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_CAL_OFFSET_2</ID> <Code>57</Code> <IDAndCode>IOUT_CAL_OFFSET phase 2 (0x01) [0x39]</IDAndCode> <ValueText>0.0000 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xE000" /> <ValueNumeric>0</ValueNumeric> <ParameterType>CurrentCalibration</ParameterType> <ParameterCategory>Calibration</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_OC_FAULT_LIMIT_2</ID> <Code>70</Code> <IDAndCode>IOUT_OC_FAULT_LIMIT phase 2 (0x01) [0x46]</IDAndCode> <ValueText>52.00 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF0D0" /> <ValueNumeric>52</ValueNumeric> <ParameterType>Current</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>IOUT_OC_WARN_LIMIT_2</ID> <Code>74</Code> <IDAndCode>IOUT_OC_WARN_LIMIT phase 2 (0x01) [0x4A]</IDAndCode> <ValueText>40.00 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xF0A0" /> <ValueNumeric>40</ValueNumeric> <ParameterType>Current</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>OT_FAULT_LIMIT_2</ID> <Code>79</Code> <IDAndCode>OT_FAULT_LIMIT phase 2 (0x01) [0x4F]</IDAndCode> <ValueText>150 °C</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x0096" /> <ValueNumeric>150</ValueNumeric> <ParameterType>Temperature</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>OT_WARN_LIMIT_2</ID> <Code>81</Code> <IDAndCode>OT_WARN_LIMIT phase 2 (0x01) [0x51]</IDAndCode> <ValueText>125 °C</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x007D" /> <ValueNumeric>125</ValueNumeric> <ParameterType>Temperature</ParameterType> <ParameterCategory>Limits</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_IOUT_2</ID> <Code>140</Code> <IDAndCode>READ_IOUT phase 2 (0x01) [0x8C]</IDAndCode> <ValueText>40.19 A</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xE283" /> <ValueNumeric>40.19</ValueNumeric> <ParameterType>Current</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_TEMPERATURE_1_2</ID> <Code>141</Code> <IDAndCode>READ_TEMPERATURE_1 phase 2 (0x01) [0x8D]</IDAndCode> <ValueText>76 °C</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xEA5E" /> <ValueNumeric>76</ValueNumeric> <ParameterType>Temperature</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_VIN_2</ID> <Code>136</Code> <IDAndCode>READ_VIN phase 2 (0x01) [0x88]</IDAndCode> <ValueText>11.969 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0xD2FE" /> <ValueNumeric>11.969</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>READ_VOUT_2</ID> <Code>139</Code> <IDAndCode>READ_VOUT phase 2 (0x01) [0x8B]</IDAndCode> <ValueText>0.925781 V</ValueText> <ValueEncoded xsi:type="PMBusWord" Hex="0x01DA" /> <ValueNumeric>0.92578125</ValueNumeric> <ParameterType>Voltage</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_CML_2</ID> <Code>126</Code> <IDAndCode>STATUS_CML_2 [0x7E]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_INPUT_2</ID> <Code>124</Code> <IDAndCode>STATUS_INPUT_2 [0x7C]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_IOUT_2</ID> <Code>123</Code> <IDAndCode>STATUS_IOUT_2 [0x7B]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_MFR_SPECIFIC_2</ID> <Code>128</Code> <IDAndCode>STATUS_MFR_SPECIFIC_2 [0x80]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> <Parameter> <ID>STATUS_TEMPERATURE_2</ID> <Code>125</Code> <IDAndCode>STATUS_TEMPERATURE_2 [0x7D]</IDAndCode> <ValueText><EMPTY></ValueText> <ValueEncoded xsi:type="PMBusByte" Hex="0x00" /> <ParameterType>Bitmask</ParameterType> <ParameterCategory>Status</ParameterCategory> <Page>255</Page> <Phase>1</Phase> <CustomIndex xsi:nil="true" /> </Parameter> </Parameters> <Other> <Custom_Commands> <READ_VTRACK_REG> <Enabled>false</Enabled> <Label>Vtrack</Label> <Gain>1</Gain> <Offset>0</Offset> <Reference>2</Reference> </READ_VTRACK_REG> </Custom_Commands> <UCD31XX_CLA_User_Data /> </Other> <Custom xsi:type="CatfishProjectData"> <Save_In_Offline_Mode>false</Save_In_Offline_Mode> <Write_To_NVM_Pending>true</Write_To_NVM_Pending> <Pin_Strapping_Info> <MSEL1> <R_Divider_Code>0</R_Divider_Code> <Rbot_Code>0</Rbot_Code> <Resistor> <Resistor_Top>0</Resistor_Top> <Resistor_Bot>0</Resistor_Bot> </Resistor> <FSW>275</FSW> <Compensation_Config> <ILOOP_GAIN>-1</ILOOP_GAIN> <VLOOP_GAIN>-1</VLOOP_GAIN> <Rbot_Code>255</Rbot_Code> <FSW>-1</FSW> <RDiv_Code>255</RDiv_Code> </Compensation_Config> </MSEL1> <MSEL2> <R_Divider_Code>0</R_Divider_Code> <Rbot_Code>0</Rbot_Code> <Resistor> <Resistor_Top>21500</Resistor_Top> <Resistor_Bot>4640</Resistor_Bot> </Resistor> <Number_Of_Slaves>0</Number_Of_Slaves> <TON_RISE>0</TON_RISE> <OC_Fault_And_Warn> <IOUT_OC_FAULT_LIMIT>52</IOUT_OC_FAULT_LIMIT> <IOUT_OC_WARN_LIMIT>40</IOUT_OC_WARN_LIMIT> <TON_RISE xsi:nil="true" /> <Number_Of_Slaves xsi:nil="true" /> <Max_OC_FAULT_LIMIT>52</Max_OC_FAULT_LIMIT> <Min_OC_FAULT_LIMIT>52</Min_OC_FAULT_LIMIT> </OC_Fault_And_Warn> </MSEL2> <VSEL> <R_Divider_Code>0</R_Divider_Code> <Rbot_Code>0</Rbot_Code> <Resistor> <Resistor_Top>0</Resistor_Top> <Resistor_Bot>0</Resistor_Bot> </Resistor> <VOUT_COMMAND>-1</VOUT_COMMAND> <VOUT_MAX>-1</VOUT_MAX> <VOUT_MIN>-1</VOUT_MIN> <VOUT_SCALE_LOOP>0</VOUT_SCALE_LOOP> </VSEL> <ADDRSEL> <R_Divider_Code>0</R_Divider_Code> <Rbot_Code>0</Rbot_Code> <Resistor> <Resistor_Top>0</Resistor_Top> <Resistor_Bot>0</Resistor_Bot> </Resistor> <Slave_Address>0</Slave_Address> <Sync>Auto</Sync> <PHASE_SHIFT>0</PHASE_SHIFT> <INTERLEAVE>0</INTERLEAVE> </ADDRSEL> <Pin_Strapping /> </Pin_Strapping_Info> </Custom> </Device> </Devices> <Sequencing_Config_V1> <Show_Warning_For_Circular_Rail_Dependencies>true</Show_Warning_For_Circular_Rail_Dependencies> <Traces /> <Int_Rail_Defs> <RailDefinition> <Part_ID>TPS546D24A</Part_ID> <Address>36</Address> <Name>Rail #1</Name> <Page_Index>0</Page_Index> <Color /> <Ext_Tracking_Mode>None</Ext_Tracking_Mode> <Control_Line>1</Control_Line> <Ext_Tracking_Custom_Source_Name /> <Operation_Event_Times> <Start>0</Start> <Stop>0</Stop> </Operation_Event_Times> <Vout>0</Vout> <Note /> </RailDefinition> </Int_Rail_Defs> <Ext_Rail_Defs /> <Devices /> <Other_Names /> </Sequencing_Config_V1> <Use_Old_UCD92XX_CLA_Gains>true</Use_Old_UCD92XX_CLA_Gains> </ProjectData>
TPS546D24A 16384.0 Address 36 PMBus Programmer Script.csv
What very well could be happening is that the electronic load is not sourcing the output current it is programmed to. The electronic loads typically need some voltage across its terminals to source their full rated current capability. Please ensure that the measured current from the load is indeed 80A in your test setup. If not, I recommend adding load bays in parallel if possible such that each load can source say half the current with a the 0.5V bias from the output of the EVM (before even considering the IR drop on the load cable).
Regards,
Alec Biesterfeld