When operating in the PWM mode, what voltage should the enable pin be connected to?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When operating in the PWM mode, what voltage should the enable pin be connected to?
Hi,
Thank you for your question. When you want the driver to be disabled then the EN pin should be pulled to GND (0V), and when you want the driver to be enabled then the EN pin should be pulled high. The input high threshold on this pin is 2.45V (meaning the pin needs 2.45V or more to recognize the signal as high). Please pay attention not to exceed the recommended operating range of this pin (-0.3V to 10V).
Best regards,
Leslie