Part Number: BUF07704
Other Parts Discussed in Thread: BUF11704
Hi,
Our customer is using BUF07704 (6ch), but due to delivery problems, we plan to use BUF11704 (10ch) temporarily.
Since the input range of each product is different for each channel, I would like to use channels with the same input range.
And their application requires 6 channels, use IN3 to IN8 of BUF11704.
Therefore, unnecessary input terminals for CH 1 and 2 are
Vdd or intermediate voltage
Similarly, CH9, 10
GND or intermediate voltage
I think that is appropriate.
Question 1
On the data sheet
CH1 ~ 3 of BUF07704 -> CH3 ~ 5 of BUF11704
CH4 ~ 6 of BUF07704 -> CH6 ~ 8 of BUF11704
I think it's better to replace it as above, but is there a problem?
Question 2
Is it okay to input Vdd / 2 with 10kΩ x2, for example, to input an intermediate voltage to process unused terminals?
Since the input bias current is very low, I think that a larger resistance value is acceptable, but please let me know if we should be careful.
Question 3
I think each channel of BUF07704 corresponds to GMA1--GMA6 in "Figure 22. Gamma Correction Curve". Is this correct?
Or is it GMA3--GMA8 because it has a different input range?
Regards,
Hiroshi