Hello expert
For the UCD3138PFCEVM-026 evaluation board, I see in your information that the duty cycle feedforward method is used to reduce the input current THD. Is there any code for this method in the PFC source program, or is there only double closed-loop control in the source code? Because so far I have not found this piece of code in the program.
Another problem is the AC drop detection. Does it have any specific functions? Under normal circumstances, there will be moments when the voltage drops below 85V in each cycle. Or is it to detect a sudden decrease in the input voltage?
Looking forward to your reply!